Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

Vertiv Issues Recommendations for Data Center Operators to Withstand Global Heat Waves

August 24, 2022

Regular data center cooling system maintenance among short-term recommendations

Columbus, Ohio [August 24, 2022] – Record-breaking heat waves are making headlines and straining economies around the globe, with no signs of cooling down in the immediate future. Beyond the impact on human lives, extreme heat is taking a major toll on data center operations and infrastructure, from outages and disruptions at data centers in the United Kingdom to reduced production at power plants in France to concerns over water usage in drought-affected areas in the United States. Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today issued recommendations to data center operators and associated businesses to help them navigate these challenges.

To keep systems cool and help ensure data center availability, Vertiv experts recommend these immediate actions:

  • Depending on the data hall load, run as many units as possible to reduce the load on each cooling unit. Typically, an organization would run all redundant units, but if the IT load is not 100%, one should run enough units to get the per-cooling unit as close as possible. This keeps the refrigerant pressures lower so there is not a risk of trips on high pressure with the high ambient temperature. It also provides a more efficient operating point.
  • Schedule a regular maintenance plan. Vertiv recommends its customers schedule preventive maintenance quarterly. For compressor-based (DX) units, Vertiv recommends quarterly or more frequent cleaning of the condenser coils. The lack of proper and regular cleaning of the condenser coil can cause more of a reduction in the overall thermal unit capacity than the ambient temperature itself. Additionally, properly maintaining the refrigerant charge level helps to enable the design capacity and operating efficiency to function smoothly. A refrigerant charge that is too low or too high, can cause operational inefficiencies.

“The unprecedented temperatures we’re seeing across the globe are putting increased pressure on data center operators and infrastructure providers, challenging them to maintain reliability and connectivity,” said Steve Madara, vice president for thermal sales at Vertiv. “Extreme weather events underscore the importance of a robust preventive maintenance and cleaning plan, tailored to the specific conditions of an operator’s region. Data center operators may need to be prepared for operating expense trade-offs to compensate for oversizing capacity. Partnering with a qualified data center services provider is important in order to create a maintenance and services plan that will meet the demands of today’s heat waves and tomorrow’s uncertain climate.”

As the planet continues to warm and the climate crisis intensifies, extreme heat events will become even more commonplace. Short-term actions will need to be accompanied by more long-term, systemic changes in the industry.

“As an industry, we should look to and learn from regions like the Middle East, Africa and Australia, which have already adapted to high temperatures for much of the year,” Madara said. “When we do, it’s clear the status quo won’t carry us into the future. We need to reassess rooftop space planning and design our data center infrastructures to withstand higher heat loads, rethinking the placement of infrastructure systems in addition to capacity.”

  • Consider different types of cooling systems, including immersion cooling, water-free cooling and evaporative freecooling systems designed to deliver reliability and efficiency in high-temperature environments.
  • If relying on solar cells as an energy source, account for the reduction of the efficacy of solar cells as ambient temperatures increase.
  • Rather than solely relying on historical data to determine data center capacity – data that fails to account for today’s extreme temperatures – use predictive modeling.

Organizations seeking an audit of their data center cooling system or with questions about business continuity and data center preventive maintenance during extreme heat events can reach out to Vertiv experts by visiting Vertiv.com.
 

#cooling #heating #hvac #heatingandcooling #hvactech #heatwave #climatechange #drought #savesoil #consciousplanet #datacenter #cloud #technology #cloudcomputing #cybersecurity
  

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com

Related Articles

Partner Login

Language & Location